This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL431: PIN2 internal connection issue

Part Number: TL431

Hi Bu:

i would like to know the internal connection of Pin2 in the SOT23-5 package like below picture, as the description of d/s, it is connected to the substrate .

Is the substrate internal connection electrically ? Can I think the PIN2 is floating internally ?

As customer's system requirement , there is the high voltage on the CATHODE , they don't expect the big voltage gap between the CATHODE and PIN2.