Hi team,
In my customer's project, LP5562 is used to drive a RGB LED.
Because of that there is no need for white LED in their system, and they need one more GPIO to control the reset signal of other chip.
They would like to consult with you. Could they use this WLED sink drive pin with the below NMOS circuit to provide a GPIO function as a reset signal for another chip?
WLED pin just need to have two status: a) 0mA sink to provide a High level for Q800; b) 18mA sink current to provide Low level for Q800.
Whether WLED sink and RGB dimming can be independent controlled?