Hello Team,
Good day. My customer is searching an IC that can do some kind of "power detection" without too much involvement of the CPU. Ideally it would detect USB Battery Charging "Charging Downstream Ports" (CDP) as well as Power Delivery capable host interfaces (ideally PD 1.0 via USB supply as well as PD 1.3 via CC lines) and just provide the information whether they can get (for example) >= 1A from the port. They already have a controller that they want to use and that should communicate with the Host directly (or via an Hub). That controller is quite fixed due to customer requirements.
Regards,
Renan