Good morning. I downloaded and installed the SIMPLIS Elements tool and their help file states that the Elements version, which is free to use, has the same capabilities as the full version with the limitation on the number of elements. I downloaded the SIMPLIS model from the TI webpage for the TPS62810-Q1 and when I run either the "startup" transient or "steady-state" transient analysis I get the error from SIMPLIS that states it cannot decrypt the file. I am now wondering if the number of elements includes each element inside a model file?