Hello,
We are using BQ25887 in our design. We don't need cell balancing feature in it, so, bit 6 in REG2A set to 0. Also, the CBSET pin left floating, and MID pin are connected to the mid point of two 33k resistor divider. The values of resistor are the same, I have double checked it. The problem is that when I check ADC readings in REG26 and REG1F, the difference between them are 100-200mV during charging(for example, 3.8780 and 4.1000). I checked that with voltmeter on the PCB, the readings the same, ADC works fine.
Can you please describe, what are the characteristics of MID pin and ADC input? In datasheet there is only one lane, about bias current.
Also, can you mention, which values of the resistor should I choose to prevent this problem? We have battery powered device, so, I can't choose too low resistance.
Thanks!