This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Customers use LM5015 and input is 24VDC, output is 17VDC and -7VDC. They found the inrush current of transformer primary side is about 3.88A when start-up. The waveform is shown as below. What is the maximum current of the internal mosfet? Does it have risk? Any suggestion? Thanks
I will need to follow up the team.
I need to understand if current limit is active in startup or changes value.
Seems the current is exceeding device HS current limit.
In addition, can you please provide schematic and power conditions under which this test was performed?
Hi Marshall,
Thanks for your reply.
Does it trigger current limit?
I have asked customer to provide schematic and sent to your email later.
Hello Yuting,
I am going to review the schematic and will get back to your comment.