Other Parts Discussed in Thread: LM5161,
Hi
I have a power supply that requires a wide input voltage (14VDC to 50VDC) and a 12V output with a max current requirement of aoubout 50mA. The main requirement was extremely low Iq. I selected the LM5161 for this and achieved most of the requirements. I selected PFM mode of operation to achieve the lowest possible Iq. The 12Volt output drives another regulator for powering the MCU at 3.3Volt.
Upon testing the supply, I noticed that there is a steep current change when going from 24Volt to 30Volt. The change is about 5-fold as you can see from the attached table. The circuit diagram is also attached for reference.
I have been through the datasheet several times to see if I have missed something, but I cannot explain the increase in current. The current measurements were taken with the MCU in idle mode, consuming a constant current in all measurements.
The application requires extremely low supply currents as hundreds of nodes needs to be powered over a distance of 30+ kilometers and 1mA extra current means a few kilometers less that can be attained.
Your help will be appreciated.
Best regards
Chris