Other Parts Discussed in Thread: TPS61098, TPS61099
Hello,
Our customer is looking for a way to get higher efficiency by using TPS613222A, so I am running WEBENCH to know the most effective inductor to take. Because the inductor is the one of the parameter to fix the switching frequency, larger the inductor lower the switching frequency. Then finally the customer is going to achieve higher efficiency by taking lower switching frequency.
However WEBECH do not recommend higher than 2.2uH inductor whereas the datasheet specify TPS613222A is able to take up to 13uH inductor.
Could you please let me know if TPS613222A bans larger than 2.2uH inductor. Our customer test condition is Vin=3.3V, Vout=5V, Iout=30mA.
Best regards,