This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDO dual channel selection

Other Parts Discussed in Thread: TLV767

Hi all,

I need to select an LDO dual channel:

  • Vin<5~6V , Vinmax= 9V;
  • Vout 1=3.3V
  • Vout 2=1.8V

Solution should be in small package (e.g. qfn 8/14).

Have you got any suggestion?

BR,
Nicolas

  • Hi Nicolas,

    There are several LDOs that you can use within the specs you provided. However, if you can provide more information I could provide a better solution (i.e. Iout, application of LDO).

    Also, is the small package a must? There are some dual channel LDOs i.e TPS767D3TPS73HD3, that have the option of fixed outputs of 1.8V and 3.3V, however, the packaging size is not as requested.

    Best,

    Edgar A.

  • Hello Nicolas,

    Another option is two small LDOs like TLV767. They are 2-mm x 2-mm each. 

    One of the drawbacks of a dual LDOs is that the total dissipation can cause the device to become quite hot.

    ~ Aaron