This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello E2E team
my question is related to the device with ordering Code TPS628692CRQY:
Does that mean, that the PG variant has only one fixed I2C address or how to covercome this problem?
Thanks in advance
Thomas Sagcob
Mentor Graphics
Hello Thomas,
Could give me a power tree here ?
Do you want to put the I2C connections in parallel or the output of the devices in parallel ?
Thanks,
Dorian
Hi Dorian,
4 devices are connected to identical I2C bus should output 4 different voltages from 1,2V to 1,8V up to 6A to supply 4 FMC cards on Vadj rails.
Regards
Thomas
Hello Thomas,
If you select the TPS628692CRQY, you will have access to the PG functionality and not the VSET/VID.
This differentiation needs to be fixed in the datasheet.
I would suggest we continue this discussion by private message/ email.
I send you a friendship request.
Thanks,
Dorian
Hello Thomas,
As we are now discussing about your design requirements and how we can address them via email, I will close this thread.
If you want to reopen it or if you uhave furrther questions, please reply below.
Thanks a lot!
Regards,
Dorian