Hi there,
From the spec, when b125611d is over-current, BATFET_DIS bit is set to 1. So I poll it every 10seconds to check if b125611d is over current. But occasionally, this bit is set to 1, about several hours, and I do not think b125611d is over current. I use DC supply to power it. Do you have any idea about it?
The words come from the spec image.
With I2C, when the BATFET turns off due to over-current, the device sets the BATFET_DIS bit to indicate the
BATFET is disabled until the input source plugs in again or one of the methods described in the BATFET Enable
(Exit Ship Mode) section is applied to re-enable BATFET.
![]()