Other Parts Discussed in Thread: TPS2116
If I have a TPS2113A device with these initial conditions: #EN=0V, VIN1=0V, and VIN2=0V, and then I switch on a 3V input to VIN1... what is the rise time on the output as it goes from 0 to 3V? I believe this is defined by tr -which indicates 3ms max. This seems slow but the datasheet mentions that the output slew rate is intentionally slow. Is there another product that will transition faster?