Other Parts Discussed in Thread: LM7481
Hello,
I am trying to understand that if i can use LM7481-Q1 for below application.
Vin: 28Vdc with 4V pk to pk 15kHz sine wave ripple, Also have a spike voltage of 120V for 1ms
Output: 28V/12A, with active rectification of 15kHz ripple
Protection: Load dump feature not required, only reverse polarity required (upto -30V continuous, and -60V peak for 1ms), so only one Mosfet will be used. Shall be able to withstand surge of 120V for 1ms & 80V for 100ms (when input voltage is above 50V Mosfet gate is not required to be driven, let the body diode conduct). Since the LM7481 is rated only upto 65V, could we use any clamp circuit with series resistor (may in ground path) to withstand the surge voltages. Plz suggest how to make LM7481 to be compatible for this surge voltage requirement application