Hello guys,
One of my customers is considering using TPS560430 for their new products.
Their conditions are the below.
Vin=24V, Vo=12V, Io=0.05A(50mA) as the maximum. So the device would be always operated in PFM mode.
They have the following questions, Could you please give me your reply?
Q1. Their load current range is 1mA~50mA. Is this current range no problem for TPS560430?
Q2. They want to get any application curves like 9.2.3 section of TPS560430 datasheet in the case that the device is operated in PFM mode.
Do you have any curve?
Q3. I think equations which described in 9.2.2 Detailed Design Procedure section are for PWM mode case.
For C and L selection, is it better to use Webench than using those equations?
Your reply would be much appreciated.
Best regards,
Kazuya.