Part Number: ISO5852S
i , I'm jaehoon kim Ph.D studeont in Seoultech university.
I use ISO5852S for the 3-phase converter. But when the gate signal should be on, it suddenly turns off and then turns on.
Please advise.
* Condition
- Topology : 3-phase converter
- Turn-on voltage : 15V
- Turn-off voltage : -5V
- Desat Fault function : don't use (Desat pin was connected to the GND)
- Situration
: All switche's Duty is 0.5 and each legs have a 120 degree phase shift.
when switch S6 is turn-on, the Gate signal of S1 is drop to the Negative voltage and re-turn on.
Please let me know how can i solve this problem.
Thank you