Hi,
my customer is using LM4040C30I as ADC reference.
And they find that their ADC digitized code would variate with the same analog input when temp changes.
So they would like to figure out what's the worst Vz variation when temp changes from like 0C to 50C.
In
6.12 LM4040C30I, LM4040D30I Electrical Characteristics
We only have Average temperature coefficient of reverse breakdown voltage maximum value at Iz=1mA for full temp range, but we are not working at this current rating, for example, Iz is 5mA in the circuit.
So how I can calculate the maximum variation of Vz with the temp change?