The prose for EN_TIMER says that it should be SET to disable the Charging Safety Timer. However the Table for Reg07 says to CLEAR the bit to disable the safety timer, which is it?
Related, it appears that my system is rebooting after 10 hours or so of runtime. In my application the battery NEVER fully charges but operates in a 70 to 80% relative state of charge range for it's lifetime. Is there anything I should do to keep my system up 24/7 while in this "never getting to full charge" mode of operation?.