Other Parts Discussed in Thread: TPS6521815,
We want to use this part for XC7Z020 but as per my study it requires I2C host which can configure (one time) the device and it will add complexity to the process.
Does TI provides/sells devices after configuration as per our application (specific for zynq 7000) or it is on customer side? Does it have different part number?
Also can you suggest any specific integrated PMIC which can be used for zynq 7000 SOC (1V, 1.5V and 1.8V) with power sequencing feature?
Thanks,
Jaimin