This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3481SEPICEVAL: Imax - SEPIC current limit behavior

Part Number: LM3481SEPICEVAL
Other Parts Discussed in Thread: LM3481-Q1, LMP8646

Hello everyone,

We are using the LM3481-Q1 in SEPIC topology in our designs.

Vin=7-24V
Vout = 12V
Iout=0.75A - set by Rsen to 0.063 OHM
f=1Mhz

I want to ask about the Iout behavior we encounter. When I choose Rsen that defines Iout to be 750mA, then why when Vin=12V the output current is indeed 750mA, but when Vin=7V, Iout can't be set to 750mA, going above 200mA will lead to Vout drop. Moreover, when Vin=24V, I can draw 1.2A (when Rsen was set to supply 750mA). So why Iout varies with Vin, and why it allows me to exceed 750mA which is the limit set by Rsen.

The current is drawn by adjustable DC load.

Thanks.