Part Number: BQ40Z50-R3-DEVICE-FW
I would like to check the expected behavior for one of the SMBus low conditions on bq40z50.
When bq40z50 sends the data to the host, in the 5th byte, the clock was pull low intentionally for 320uS, would bq40z50 still able to complete sending for 6th byte and 7th byte data to the host?
Please correct me if I am wrong, from what I have found, bq40z50 comply with SMBus spec. V1.1. In the spec. it states that the Timeout for 100Mhz communication is 25ms (max). So as long as each data could complete within 25ms, bq40z50 should be able to send the correct data to the host. Is that correct?