Is it possible to use a connector to plug simulteanously the 5 wires of a 4-cell batteries on a circuit with BQ29400 and BQ2085?
BQ29400 documentation says "To prevent incorrect output activation the following connection sequences must be used. 4-Series Cell Configuration
· VC1(=VDD) ® VC2 ® VC3 ® VC4 ® GND or
· GND ® VC4 ® VC3 ® VC2 ® VC1(=VDD)"
But is this really mandatory or can we plug all-at-once? (much easier to implement in production and maintenance...)
Thanks for answer
Francois