Other Parts Discussed in Thread: TPS53315, TPS548A20, TPS25982
Hi ,
I am using TPS53315 in my design. I sharing the webench simulation that I used to check my design here.
Vin=12V, Vout=5V, Iout=8A, fsw=500kHz, SS=2.8ms
1. As per the formula provided in datasheet for inductor calculation, i get L=2.2uH. But in webench simulation I don't find any 2.2uH option to select. Which inductor value should I consider
2. Also as per formula, if OCP is 15A the calculated RTRIP value as per datasheet should be 76.57kohm. But in webench only resistor values from 65.3kohm to 67.96kohm is present. Which value should i consider.
3. Also I have added extra output capacitors because I will be hotplugging SATA HDD device which will have 5V output of this regulator connected to it. In the earlier board designed with this regulator, because of the sudden inrush current the output voltage would drop to mV and then again get stable when HDD was connected.
Attaching the link for conversation regarding this issue with TI Engineer.
4. Also I have attached my schematics for reference. There I have also added additional bulk capacitors near the SATA connectors to avoid any sudden inrush current issue. Will these additional capcitors cause instability issue.
5. Also can you please provide a proper ripple injection circuit value for my circuit so that I don't face any stability issue.