I'm trying to figure out how large of an inductor value can be used with the LM60430-Q1 when the max load current is under 500 mA?
Using Webench, it recommends 10 uH, while the Quick Start calculator reports 60 uH. I'm worried that 60 uH is too large for the internal compensation, but 10 uH seems too low. I expect the converter will be in PFM mode with this light load, but want to see if I can raise the PFM frequency some.