Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

From 220VAC to 12V-48VDC converter

Other Parts Discussed in Thread: UCC28951, UCC28950, UCC21520

Hi,

We are making a ac dc converter of 3.5KW. AC input is 220V. Actual output is either 12V or 24V or 48V. Only one is selected. Max current is 60A. This is battery charger. ZVS PSFB is suggeated. But output is limited.

We have looked at multiple options, but cannot find any till now. Please help as soon as possible. 

Till than, we are looking for two phase buck converter with two device in parallel. Losses may be on higher side, but solution has highest priority.

Vikas Dabas