This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25600: ucc25600

Part Number: UCC25600


Hi,

In your datasheet I heard that UCC25600 is suitable for power less tha 1KW. But in my point, it's only a cotroller IC and should be suitable for more higher power.

Currently I want to design a LLC circuit with 3.5KW, did the IC fit?

Also in your refer design, the IC is primary side cotrolled, so an opto-coupler is needed. But in my design the IC is secondary side cotrolled , so what's the feedback circuit? Can you give me a refer circuit?

Thanks.

  • Hi,

    UCC25600 can support full bridge LLC also which can handle 3.5kW, here is an reference circuit.2570.Schematic Prints.pdf

    And UCC25600 is recommended to located on primary side as the circuit. 

  • Hi,

    Thanks for your reply and schematic. In my opinion, if the driver ic is boostrap, the UCC25600 should be primary. But I driver the MOSFET with driver transformer, then the UCC25600 can be located in the secondary side. What's your opinion? If I use the UCC25600 in the secondary side, what's the risk? And also can you give me a feedback cirucit? I think the current mirror is useful, how do you think about it?

    Thanks.

  • Hi, Fleming

    You are correct, In theory, UCC25600 can be located in primary side or secondary side if the driver circuit with driver transformer.

    But I still recommended to put UCC25600 on primary side since I don't have a feedback circuit to you. And there is no further benefit compare with putting UCC25600 on primary side.

    Yunsheng