This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62840: Current consumption increase for very close of Vin and Vout...

Part Number: TPS62840


Dear Sirs,

My customer use TPS62840 for 3.3V output to their system.

He found while the system in standby mode and the TPS62840 Vin is 3.36V~3.39V, the current consumption will increase 600~900uA.

If the Vin is higher than this period, the system current will return to normal.(~0.02mA).

Is this symptom normal or not?

The customer test report as attached.

Thanks.

TPS62840耗電問題_20210312.pdf

  • Hi Peter,

    Thank you for your question.

    This behavior is intrinsic of the device operation, and it is present near the border between 100% Mode Operation and PFM Mode. In this region small variations of VIN / VOUT (for example the voltage ripple), can toggle the mode of operation of the device that, working in a not well defined condition, periodically starts switching, increasing the overall current consumption.

    As soon as you exit this critical region (either increasing or decreasing VIN), the device returns in a defined operation mode, consequently reducing also the current consumption.

    The problem can be minimized increasing CIN/COUT in order to reduce the voltage ripples but cannot be eliminated, since it is intrinsic to the converter control. 

    Please ask again if you need further support.

    Thanks,

    Stefano

    All information in this correspondence and in any related correspondence is provided “as is” and “with all faults”, and is subject to TI’s Important Notice (http://www.ti.com/corp/docs/legal/important-notice.shtml).