This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54335A: Output pin (PH, pin 3) is shorted to GND

Part Number: TPS54335A


1. It is a buck converter with input voltage 8 to 18V and output is 5V in our PCB. Maximum current in our system is 1.5A
2. We observed the output pin (PH, pin 3) is shorted to GND.
3. Around 10 TPS54335A IC got failed.

4. We need your immediate support for this issue.