With respect to the datasheet i have understood that each cell can be balancing by using Cell balancing registers,
Each bits (D0 to D4) in the CELLBALx registers, corresponds to each cell from cell 1 to cell 15
In my case , Only 13 cells are connected as per the datasheet page no 42, VC14-VC13 and VC9-VC8 are shorted,
Query Description
1.For 13 cell configuration which two bits should be ignored in the CELLBALx registers
1.In order to balance CELL 9 and CELL 13 which bits present in CELLBAL x register should be used?
2.With respect to my understanding, bits CB10 and CB15 should be used? But it is not giving expected outcome
Please correct my understanding