This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5066: GATE pin is not working after the output is shorted and come back to normal

Part Number: LM5066

Hello TI experts,

my customer is now designing LM5066 for their power supply, and made 1st PCB, there is problem.

overcurrent protection works well. if they put overcurrent condition, the power delivery stops, and back to normal current, the power delivery start again.

but in short protection, it does not come back to normal.

we short CN5 pin, the power delivery stops. but after release the short in CN5, power delivery does not start again. (actually we cannot see the output from GATE(pin2) pin.)

here is the schematic below. can you check it for our problem?

(CL(pin22) is connected to VDD, to set the overcurrent threshold to be 26 mV)

test condition is as below;

  - input voltage : +52Vdc ~ +53Vdc

  - output current load : 0A ~ 1.8A

please check this issue. Thanks.

Best regards,

Chase