Other Parts Discussed in Thread: TPS51396,
Hi team,
My customer would like to know does TPS568230 p2p and Bom 2 BOM with TPS51396?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Paul,
What is the input voltage? What is the frequency and operation mode setting?
TPS568230 is a 18Vin max, EN max=4V, three frequency selection and non-latch for fault. While TPS51396 is a 24Vin max, EN max can be up to 6V, only 580KHz frequency setting and latch for OV&UV fault condition.
They are P2P. But B2B needs to according the application.
Thanks,
Lishuang