Other Parts Discussed in Thread: TPS54561, TPS54560B
Hi Team,
Good day.
Customer want to confirm the following.
1. In the photo customer want to control the output voltage by adding a digital potentiometer in place of R2 (want to control the output voltage from 5V To 15V). Is this possible for the design in the datasheet without changing other external components? According to them, values of the inductors and capacitors changes when tried using the the webench
2. Customer also want to use 24 Voltage as an input voltage and 4-5 Amperes as output current
Thank you.
Regards,
Maynard