This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74610-Q1: Is it possible to extent continuous Vin beyond -45V?

Part Number: LM74610-Q1
Other Parts Discussed in Thread: LM5050-1

Hello all.

I want to build a high-current reverse input protection circuit that can withstand up to -65V continuous reverse input.

I know that what follows is just a crazy, not feasible idea, however I would like to share it with you: LM74610-Q1 can withstand reverse voltages up to -45V between anode and cathode pins. We could  overcome that limit by inserting a suitable resistor in series with Anode pin and a 39V zener between Anode and cathode. Unfortunately, Anode pin is also used for sensing the mosfet drain-source voltage during reverse polarity operation so I expect that this resistor-zener addition will prevent normal operation.

Perhaps TI could offer another version of this IC with separate Vcc and voltage sense pins. Unitl then, I guess that what I am proposing above wouldn't work at all. Disappointed

Next option is to use LM5050-1, by connecting a diode in series with Vss pin, per LM5050-1 datasheet page 20. Datasheet says it works up to -48V but I see no reason no to operate up to +/-75V. Is it a recommended solution?

Regards

Dimitrios