I am using TPS54062 to design a buck convertor with Vin (nom) = 24V, Vout=5V, Iout=20mA max.
After designing and simulating the entire circuit on Webench, I physically assembled the circuit with the exact same component values.
The output voltage comes out to 5V as designed but it drops to 0.5V when load (220 ohm resistor) is connected.
I am attaching the Webench design report to show the component values that I have used. Please help.