This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61495-Q1: Need VOH details

Part Number: LM61495-Q1

Hi,

Please let me know the VOH value for RESET pin of LM61495-Q1.

  • Hi,

    Edit:

    The RESET pin is an open drain output used to tell the operational status of the device.

    The RESET pin has a maximum voltage rating of 20V. This should also be considered the VOH value of the RESET pin. 

    Figure 8 also provides a timing diagram that shows RESET with a pullup resistor to an voltage rail <20V. 

    Jimmy