Part Number: TPS61288EVM-064
Other Parts Discussed in Thread: TPS61288
Hi sir,
I use evaluation board tps61288 evm-064 now.
The circuit is changed so that the output voltage becomes 6V.
If the output load of the power source is only the load (12 ohms), the input voltage is driven even if the input voltage is 2.0 V,
but if the output load of the power source is connected to the load (12ohm) in parallel with the cap 200uF, the circuit will shut down when the input voltage becomes 2.7V or less.
Can you tell me to adjust which parts value in the circuit, so that the Min 2.0V can drive this requirement.

Thanks.