This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63010: Reverse current protection

Part Number: TPS63010

Dears

If the TPS63010 configurated as 3.3V output, and add a 3.4V on the output of TPS63010, will there have some problem or damage?  if Yes, do we have a similar buck boost device can support this condition?  in the application we have 2 DCDC output connect together to support the load.

Thanks

Jun Shen