Other Parts Discussed in Thread: BQ7718, BQ2947, BQ7716
Hello,
I have designed my first LiPo battery circuit and I need some input to check if this circuit is safe and protect the LiPo and the circuit from any damage. Please take a look at the snippet:

I use two LiPo batteries and the input voltage is converted to my supply voltage (this part is not shown). The circuit doesn´t contain a charging circuit, so I skipped a battery guard with overvoltage protection and simply use the BQ2961 (BQ296106) because of its Undervoltage protection.
NOTE: I don´t want to use the internal regulator of this chip, so I disable it (I think I disable it - correct me if this part is wrong) to save a little bit of current. The MOSFET "Q201" is used as reverse polarity protection and I use "F201" as thermal protection. The parts behind the fuse are used by the battery voltage measurement circuit.
So my circuit contains:
- Reverse polarity protection
- Thermal protection
- Undervoltage protection
Do I need other safety features to protect my circuit and my LiPo battery?
Thank you for your help and your ideas
Best wishes