The question i have is about the temperature limits OTC and OTD.
The Technical Reference Manual states that for the OTC treshold
When the maximum cell temperature is greater than or equal to this threshold for Protections:OTC:Delay seconds, the protection is triggered. Note that charging does not need to be occurring for this protection to trigger. I
And with automatic FET control we can switch of the charge fet via the OTC.
But When the OTC and OTD thresholds are at different values, we can have a situation that the discharge FET is on and the charge FET is disabled.
This will result in the charge FET being possibly damaged, as we will discharge over the body diode of the charge FET.
My problem is why can the OTC trigger when we are discharging.