Hi,
We chose to use BQ7791501 for battery pack protection and cell balancing. We will use 32pcs of 4900mAh Li-ion cells so that 8pcs will be in parallel and four of these packs in series, making a 39.2Ah / 16,8V battery pack. Charger voltage is 16,8V and max current 17A.
33ohm resistors were chosen to set the balancing current to ~50mA as on the datasheet example. Current sense resistor of 1mohm is selected for a 35A maximum discharge current and 20A charging current.
What I haven't understood is why there are two different OCD values, OCD1 and OCD2? For example in our case the OCD1 threshold is -35mV so with a 1mohm current sense resistor the voltage will go below the limit at 35A if I'm correct. OCD2 voltage threshold of -60mV will never be achieved.
Please review the schematic attached.
Kind regards,
Olli-Pekka