Hi ,everyone
I try to set dataflash in bq27541-V200. I don't know about some values whether appropriate according to my application. In the document "Configuring the bq27541-V200 Data Flash", Give the default values but the details about the calculation.
Max Res Factor : 15 num Min Res Factor: 3 num
Ra Filter: 500 num
Max DeltaV: 200mV Min Delta: 0 mV
Max Sim Rate: 1 C/Rate Min Sim Rate: 20 C/Rate
Ra Max Delta: 44 mOhms
DeltaV Max Delta: 10mv
Max IR Correct: 400mV
My application: Battery pack: 2S1P Capacity: 1620 mAh. Standby current: 20 mA Normal operation: 50ms pulse width with curent 10A(peak current: 14A) along with 2A.
Best regards
Jason