This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS709: EN pin of TPS70933DRV

Part Number: TPS709

Hi team,

According to the datasheet of TPS70933DRV, the EN pin can be left open as chip enabled. 

In my application, the input voltage is 12~25V. From reliability & EMS point of view, what is the best way to deal with EN pin? is there any concerns to left open?

Best regards.

Wendy

  • Hi Wendy,

    You can leave the EN pin floating.  If you want to tie it to Vin externally, you will need to use a voltage divider to reduce the voltage from the Vin rail.  A divider ratio of 6/25, maximum, should work from Vin to the enable pin.

    Thanks,

    - Stephen