Part Number: LM5116
Hi
Does LM5116 have the below functions?
- Input Overvoltage LockOut
- Output Overvoltage Protection
If there is no function, can you recommend an additional external circuit?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5116
Hi
Does LM5116 have the below functions?
- Input Overvoltage LockOut
- Output Overvoltage Protection
If there is no function, can you recommend an additional external circuit?
Thanks
Hi
Thank you for your support.
I have additional questions.
1. Thermal Protection
: I know that the LM5116 has thermal protection function.
It will probably be a thermal protection at over 150 degrees.
Is there any way to adjust the protection setting temperature?
For example, is there any way to make temperature protection at 85 degrees?
2. Output Voltage Protection
: If the output voltage increases when the FB pin is open, can LM5116 protect it?
Thanks
Hi David,
1. No adjustment is possible externall to the thermal shutdown. Consider using a separate thermal monitor IC if needed.
2. If FB is open, the contorller does not have output voltage information for regulation and COMP will go high.
Regards,
Tim