Other Parts Discussed in Thread: TPS40210, LM5155, LM5176
HI,
I want to design a programmable PSU with input range of 4.5V to 22V and a variable output 0 to 5V with current of about 2~4A[maximum total power 20W].
the Vout voltage will be controlled via changing the FB voltage with an opamp.instead of the fixed votlage dividers.
The PowerDesigner tool has some options with TPS40211, am i on the right track?
Thanks!