The LM27222 LEN pin disables turn on of the low side FET. Is the high side FET drive still enabled and controlled by the PWM input? Operation is not explicitly stated in the data sheet.
Thanks,
Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The LM27222 LEN pin disables turn on of the low side FET. Is the high side FET drive still enabled and controlled by the PWM input? Operation is not explicitly stated in the data sheet.
Thanks,
Mark
Hello Mark,
The LEN pin input is a disable/enable for the low side driver output. The PWM will control the high side driver output. With a single PWM input, a low on PWM results in the low side driver high, there may be some conditions such as DCM operation or system shutdown where you desire both driver outputs to be low. The LEN signal allows for this driver output state.
Confirm if this addresses your questions, or you can post additional questions on this thread.
Regards,