This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65631W: Swire protocol control power IC for OLED

Part Number: TPS65631W
Other Parts Discussed in Thread: TPS65631, TPS65632,

Team,

Do we have Swire protocol control power IC for OLED and also meet below requirements?

  1. Dual output:
  • Fixed positive voltage output
  • Positive voltage range can be 4.5V to 5.5V
  • digitally programmable negative output
  • negative output adjusted by Swire control
  • negative voltage output range -2.4V to -6.4V
  • pos/neg output current 300mA maximum
  1. input voltage range 2.9V to 4.5V

Regards,

Roy