Other Parts Discussed in Thread: LMG1205,
Hi,
I'm working with the LM5113 connected as below:
I'm using the high side driving section to drive a E-GaN to push current to a load.
I have no problem in driving a resistive load, i tried to drive with 18 A current peaks with no problems.
I have to test the response to the load short circuit, but when i connect a short circuit instead of a resistance, i experience a LM5113 failure. After this failure i measure the impedence beetween HS and HOL (that is connected to HOH in my circuit) pins of 2 ohm instead of 100kohms in normal condition.
Could you tell me what is going in failure? Have you some idea to let the LM5113 survive to load short circuits?
Thank you, regards
Mattia