Other Parts Discussed in Thread: BQ25792, BQ25798, BQ25798EVM
1) I want to use D + / D–Detection so that the Unknown Adapter is set to the default setting. Should I set D + / D- to open?
Or according to the table below
・ GND connection via D + = 1 MΩ resistor
・ PullUp to D- = 3.3V or higher
Should I do that?
In that case, what is the PullUp resistance value of D-?
Is it okay to pull up with REGN?

2) If VBUS is turned on with ILIM_HIZ = Low when the battery is not connected, the VSYS voltage will be about 3.2V. I thought that the output would be 0V because the converter is not operating. Could you please tell me the reason?
3) If I start charging with the battery disconnected, the following QA-like shutdown occured.
At the end, Jeff said, "This week I will be evaluating new versions of the BQ25792 with some additional features." So I want to know what the result.
Also, Jeff has proposed adding a capacitor larger than 470uF as a countermeasure, but I would like to know the reason why 100uF is not good.
Best regards,
Kagawa