Hi Team,
The power input voltage is 6~7V, the input current is about 0.9A, and the output voltage is 12V. The currently selected tantalum capacitors, C4 and C5 are 220uF/16V, and the inductance is 100uH. At present, customer find that the capacitor and the inductance are very hot.
Could you help to confirm whether there is a problem in SCH.