This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Request for LED Driver IC Recommendation

Hi, Support Team

Customers are looking for an inexpensive LED Driver IC.

Attached data is the datasheet of the LED to be used.

RGB LED_L-C19F1RGBCT-CA-XM1.pdf

And the picture below is the actual color to be applied.

I want to operate the LED under the following conditions.

1. The LED status indicator must support the following RGB code :

Blue Hex : #008CFF

Red Hex : #FF0000

2. The LED status indicator must have the ability to fade consistently to/from 0% and 100%.

Please recommend an LED Driver IC that can operate as described above.

Thanks.

Regards,

MJ

  • Hi MJ

    We have several products which can meet your request. So could you please provide more information?

    1. what about the maximum and minimum current do you want?
    2. how much bits does the PWM dimming need? or whether you want to using analog dimming?
    3. how much pwm frequency do you want?

    Best Regard

    Monet Xu