Other Parts Discussed in Thread: LM5121, TPS43061, TPS43060
Hello TI experts,
my customers consider the boost controller of TI product.
first they consider LM5122 and LM5121, but i don't know the difference exactly.
- LM5121 : have good efficiency at light load, and have adjustable current limit.
- LM5122 : phase interleaving.
1. what is more difference between these 2 devices?
2. compare these 2 device and TPS43601, what is the good point of TPS43601?
3. what is the reason of the cheap price of TPS43601 compare to LM5122 and LM5121? (almost half price)
4. can you recommend the best IC that suitable for our condition?
- input : 24Vdc, output : 30Vdc
- current : max 10A
- others : need overvoltage and short protection
please check these issues. Thanks.
Best regards,
Chase